The price includes applicable sales taxes.

XW Conduit Box

(0) No Reviews yet

Product Description

Product Description

The XW Conduit Box mounts directly to the bottom of an XW inverter to safely protect end-users from inadvertent contact with wiring or connections. The XW Conduit Box is bundled with the Power Distribution Panel and the XW Connection Kit, however, it is also available for order on its own. The Conduit Box is easily secured with two screws provided on the bottom of the inverter. The bottom flange of the conduit box can then be attached (fasteners not provided) to the wall to complete the installation. The front panel of the conduit box can be removed by removing the two screws on the front, allowing ample space to make all necessary wiring connections. In multi-unit installations, the sides of adjacent conduit boxes can be removed to create an effective raceway with lots of volume to run AC and DC inverter cabling. The conduit box also includes multiple cable strap points, allowing the final installation to look clean and professional. In addition, an internal sheet metal barrier is included to keep communications wires separate from AC and DC power wires.
SKU: 865-1025-01
$208.56

Ratings & Reviews

No reviews available

Be the first to Write a review